AXIS#.HOME.AUTOMOVE
Description
AXIS#.HOME.AUTOMOVE selects if the axis will start the configured homing move when the axis is enabled.
Value | Description |
---|---|
0 | The axis will never start a homing move when the axis is enabled. |
1 |
The axis will start a homing move when the axis is enabled. This homing move is skipped if: The axis is already homed The axis is not in position mode (AXIS#.OPMODE = 2) The axis is not in service mode (AXIS#.CMDSOURCE = 0). |
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 to 1 |
Default Value |
0 |
Data Type |
Integer |
See Also |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.HOME.AUTOMOVE | 0x5008 | 0x4 | USINT | - | - | RW | False |
AXIS2.HOME.AUTOMOVE | 0x5108 | 0x4 | USINT | - | - | RW | False |
Related Topics
Homing